MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDL noise and maximum accuracy

In my system that found the heading angle using the LIS3MDL sensor, the maximum error value was 3 degrees using the ellipsoid calibration method. Also, although I used the sensor in low noise mode, I saw that the data in Matlab graphics was very wavy...

Problems to communicate with steval-mki193v1

I have a steval-mki193a1. I tried to connect it with nordic nrf52-dk by I2C. However, the sensor cannot be successfully detected by the nordic nrf52-dk board. How can I make them communicate successfully so that I can get the sensor data on computer?...

MKI109V3 Port Fault

Hello,I am experiencing a port fault issue with my Steval-MKI109v3 board which is equipped with an LSM6DSV16x sensor. Despite following the tutorial, I cannot locate the St virtual port on my device. Additionally, I have updated my drivers based on t...

FKara.3 by Senior
  • 1040 Views
  • 0 replies
  • 0 kudos

Cannot run STHS34PF80TR sensor at full speed over SPI bus.

Hello!We are using STHS34PF80 IR sensor and STM32L031F6 processor in our IR motion sensor device.In STHS34PF80 datasheet is said that SPI clock speed could be up to 10 MHz.But we can achieve clock speeds up to 250 kHz.Strange think is that we are abl...

LMehm by Associate III
  • 2592 Views
  • 4 replies
  • 0 kudos

Resolved! Question about LSM6DSO PCB design

I'm currently trying to build a custom PCB using LSM6DSO. I just have few questions about the pins I don't use. I have no need for SPI communication, interrupts and VDD, not VDDIO cuz I need to power it through my RPi. I only need I2C communication a...

Community check.png solder.png
el659 by Associate III
  • 2681 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSV SFLP

I am reading quaternions from the SFLP and converting to yaw, pitch and roll (YPR). The results are remarkably stable and accurate! I noticed though when performing some simple testing with the sensor on a breadboard and the breadboard flat on a tabl...

KWine by Senior
  • 2925 Views
  • 2 replies
  • 0 kudos

IIS2MDC always on Idle Mode

Hi!I'm exploring the X-NUCLEO-IKS02A1 with the IIS2MDC magnetometer.My purpose is read the output data, but I haven't even been able to read the temperature. I'm using I2C through PB8 and PB9 pins, and I have communication cuz' the sensor responds to...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.