2023-09-25 6:25 AM
Hello,
I'm looking to see if there is a maximum value for the sleep-to-wake interrupt register on the LIS2DE12. I do see +/- 2g, 4g, 8g, 16g as standard values, but is it okay to set a threshold value to +/-30g, 25g or 20g?
Thanks!
2023-09-28 8:00 AM
Hi @baraadalaq ,
Welcome to ST Community!
You need to stay within the FS range, so at maximum value of 16g.
If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)
2023-09-29 8:56 AM - edited 2023-09-29 8:57 AM
Thanks for the reply. Would the device become unstable past the maximum value?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.