MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error in Reading temperature using Lis3dh

 Hi everyone, I have an STM32L4 series-based board with an embedded LIS3DH sensor. I've written code to read temperature values from it, configuring all settings as per the datasheet. However, I'm having trouble obtaining the exact temperature value ...

AKH by Associate
  • 1920 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2MDL Magnetometer unable to find vdd supply

Hi I am using the LIS2MDL Magnetometer, which is connected to i2c0 on my custom board. I have enabled the respective kernel configuration for the magnetometer.CONFIG_IIO_ST_SENSORS_I2C=yCONFIG_IIO_ST_SENSORS_SPI=yCONFIG_IIO_ST_SENSORS_CORE=yCONFIG_II...

Resolved! Handling of LSM303 unused pins

Hello,have designed in an LSM303AGR to replace an obsolete NXP chip, it used in I2C mode at 3.3V, and there are twopins that is not used, i.e. pin 7 - INT_MAG/DRDY and pin 12 - INT_1_XL.Upon testing, when the complete system is in sleep mode, we have...

AGI by Associate II
  • 4877 Views
  • 6 replies
  • 0 kudos

Digital MEMS Microphone Noise Floor

Hi,I'm using an MP23DB02MM digital mic on the CCA02M2 eval board and using the PDM2PCM library. When I have no sound into the microphone the noise floor I see in the data from the PDM2PCM output is around 1,000 counts peak to peak noise. I'm struggli...

JKing.3 by Associate II
  • 5050 Views
  • 8 replies
  • 0 kudos

Resolved! ASM330LHH Frequency Measurement using the mother UNICO-GUI

Hi there,We are testing the ASM330LHH with the motherboard STEVAL-MKI193V1 and use Unico-GUI to collect data.  ODR was set to be 6667 Hz and easy configuration was used. The excitation was a 1kHz sin wave but the data saved using Unico-GUI showed a f...

Resolved! LIS2DH12 data rate

Hello,LIS2DH12 accelerometer. Datasheet AN5005 shows Table 4.Is this the speed of data transfer via the SPI or I2C interface? Or the speed of converting data into accelerations and writing this accelerations to the OUTX_H and OUTX_L registers?

MykolaLevun_0-1707283363569.png

Getting Problem sometime With LSM6DSO Acc and gyro

Hi Team , I'm using your ST acc and gyro LSM6DSOTR datasheet https://www.st.com/resource/en/datasheet/lsm6dso.pdf at sometime an acc stop sending its values can you guys please help me figure the issue  and whenever i restart then its sending values ...

ashutamar_1-1707333122862.png ashutamar_2-1707333381937.png
ashutamar by Associate II
  • 1024 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.