2024-02-09 11:06 AM
To make it more clear,
Library version: 0.19 (git tag: v0.19) Compiled with backends: local xml ip usb serial IIO context created with local backend. Backend version: 0.19 (git tag: v0.19) Backend description string: Linux dab 5.4.193-toradex #1 SMP PREEMPT Fri Oct 6 13:55:59 CEST 2023 aarch64 IIO context has 1 attributes: local,kernel: 5.4.193-toradex IIO context has 6 devices: .... iio:device1: ilps22qs (buffer capable) 3 channels found: pressure: (input) 2 channel-specific attributes found: attr 0: raw value: 4143498 attr 1: scale value: 0.000024414 temp: (input) 2 channel-specific attributes found: attr 0: raw value: 4278 attr 1: scale value: 10.000000000 timestamp: (input, index: 2, format: le:S64/64>>0) 5 device-specific attributes found: attr 0: consumers ERROR: Input/output error (-5) attr 1: current_timestamp_clock value: realtime attr 2: sampling_frequency value: 1 attr 3: sampling_frequency_available value: 1 4 10 25 50 75 100 200 attr 4: suppliers ERROR: Input/output error (-5) 2 buffer-specific attributes found: attr 0: data_available value: 0 attr 1: watermark value: 1 iio:device2: iis2mdc (buffer capable) 4 channels found: magn_x: (input, index: 0, format: le:S16/16>>0) 3 channel-specific attributes found: attr 0: raw ERROR: Device or resource busy (-16) attr 1: scale value: 0.001500 attr 2: scale_available value: 0.001500 magn_y: (input, index: 1, format: le:S16/16>>0) 3 channel-specific attributes found: attr 0: raw ERROR: Device or resource busy (-16) attr 1: scale value: 0.001500 attr 2: scale_available value: 0.001500 magn_z: (input, index: 2, format: le:S16/16>>0) 3 channel-specific attributes found: attr 0: raw ERROR: Device or resource busy (-16) attr 1: scale value: 0.001500 attr 2: scale_available value: 0.001500 timestamp: (input, index: 3, format: le:S64/64>>0) 5 device-specific attributes found: attr 0: consumers ERROR: Input/output error (-5) attr 1: current_timestamp_clock value: realtime attr 2: sampling_frequency value: 10 attr 3: sampling_frequency_available value: 10 20 50 100 attr 4: suppliers ERROR: Input/output error (-5) 2 buffer-specific attributes found: attr 0: data_available value: 16 attr 1: watermark value: 1 Current trigger: trigger0(iis2mdc-trigger) ... attr 1: watermark value: 1 trigger0: iis2mdc-trigger 0 channels found: 2 device-specific attributes found: attr 0: consumers ERROR: Input/output error (-5) attr 1: suppliers ERROR: Input/output error (-5)
Trying to work from the linux terminal (sysfs), so for example enabling the buffer with "sudo echo 1 > buffer/enable" (and similar commands) for the magnetometer I am able to obtain the data but not the timestamp, while in the case of the barometer I am not even able to enable the buffer (it says "1" is a wrong argument for the "enable" file). So I do not know how these problems are linked with the trigger and how to resolve them.
I also already tried to deactivate the trigger for the barometer (see the code below), but it then says it is not able to create the buffer. Same thing if I do not deactivate the trigger. I recall thatfor the barometer no trigger has been set-up, so maybe the problem is that I should create one instead of deactivating it... For the magnetometer I didn't try with the C++ code but from sysfs I was not able to get the timestamp and so I guess the problem will be the same if I try to work with the code.
So the questions are:
1. How can I get the "timestamp" for the magnometer?
2. How can I make the barometer work (data + timestamp)?
It's fine for me to work either from the linux terminal (sysfs) or with a C++ code.
Thanks in advance
trigger_device = iio_device_set_trigger(press_device, NULL); if (!trigger_device) { std::cerr << "Trigger not disabled" << std::endl; iio_context_destroy(ctx); return -1; }
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.