2017-11-27 9:56 PM
Hello!
I have a problem with BlueNRG chip (old one, NOT BlueNRG-MS). I made a custom PCB with STM32F407VGT6 and BlueNRG on it and try to setup. In MCU test firmware there aren't any functions that used for commutication with BLE chip. When I turn on my device, I always notice that there is a VCC voltage on IRQ pin of BlueNRG. According to documentation this means that there is some data to read. Strange! What data should I read, if I haven't sent any command?.. Ok, I read it. First send a read header and recieve this: status = 0x02, write buffer = 0x3F and read buffer = 0x After that I get this array of bytes: 0x04, 0xFF, 0x03, 0x01, 0x00, 0x01. The first question is: what is it? How should I interpret it?Next, I want to send some command and watch response. I tested HCI_Reset, HCI_Read_Local_Version_Information, HCI_Read_Local_Supported_Commands, HCI_LE_Read_Buffer_Size... Every time I get this response:
1. Header is: status = 0x02, write buffer = 0x3F and read buffer = 0x04 2. Response body: 0x04, 0x10, 0x01, 0x00Second question is: what does this response mean? Why when I send any command, I always get this?
This is my C++ code for transmiting and recieving data:
struct Header
{
uint8 status;
uint16 writeBuffer;
uint16 readBuffer;
};
Header getHeader(uint8 type)
{
uint8 status = SPIwriteAndRead(type); // read status
uint16 writeBuffer = SPIwriteAndRead(0x00) | (SPIwriteAndRead(0x00) << 8); // read writeBuffer
uint16 readBuffer = SPIwriteAndRead(0x00) | (SPIwriteAndRead(0x00) << 8); // read readBuffer
return {status, writeBuffer, readBuffer};
}
void readResponse(uint8 *buffer, uint16 size)
{
for(uint16 i = 0; i < size; i++)
buffer[i] = SPIwriteAndRead(0x00); // send dummy byte and recieve data
}
void sendCommand(uint8 *data, uint8 size)
{
for(uint8 i = 0; i < size; i++)
SPIwriteAndRead(data[i]); // send data byte
}
int main()
{
initMCU(): // init GPIO, SPI, RCC...
//---- read incomming message
uint8 responseBuffer[127] = {0};
waitForEvent(); // wait when IRQ pin of BlueNRG becomes high
while(true)
{
setCSLow(); // begin transmission
Header header = getHeader(0x0B); // send Read header
if(header.status == 0x02 && header.readBuffer > 0) // check if BlueNRG is ready and has something in its read buffer
{
readResponse(responseBuffer, header.readBuffer); // read data
setCSHigh(); // finish commutication
break;
}
else setCSHigh(); //conditions don't match, finish commutication
}
//---- at this moment responseBuffer contains 0x04, 0xFF, 0x03, 0x01, 0x00, 0x01;
//---- let's execute HCI_Read_Local_Version_Information
setCSLow(); // begin transmission
Header header = getHeader(0x0A); // send Write header
if(header.status == 0x02) // check if BlueNRG is ready
{
sendCommand({0x10, 0x01, 0x00}, 3); // opcode = 0x1001 and length of parameters = 0
setCSHigh(); // finish commutication
}
else
{
// error...
setCSHigh(); // finish commutication
while(true);
}
uint8 commandbuffer[127] = {0};
waitForEvent(); // wait when IRQ pin of BlueNRG becomes high
while(true)
{
setCSLow(); // begin transmission
Header header = getHeader(0x0B); // send Read header
if(header.status == 0x02 && header.readBuffer > 0) // check if BlueNRG is ready and has something in its read buffer
{
readResponse(commandbuffer, header.readBuffer); // read data
setCSHigh(); // finish commutication
break;
}
else setCSHigh(); //conditions don't match, finish commutication
}
//---- at this moment commandbuffer contains 0x04, 0x10, 0x01, 0x00;
while(true);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
I think I miss something... Help me please!
#bluenrg #response2017-12-02 4:13 AM
According to 'AN4494 Bringing up the BlueNRG and BlueNRG-MS devices' these bytes - 0x04, 0xFF, 0x03, 0x01, 0x00, 0x01 mean a Blue_Initialized_Event. And we see them - it is very good.
If I understood correctly these bytes 0x04, 0x10, 0x01, 0x00 - mean a hardware error with code 0 - SPI framing error (UM1865 BlueNRG-MS Bluetooth LE stack application command interface (ACI)).
My SPI setup is correct:
CR1 = 0x00000344
SR = 0x00000002
CRCPR = 0x00000007
I2SPR = 0x00000002
Other registers are = 0
I ask you: WHY your IC gives an error?
I tested two IC and result is the same!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.