2016-01-29 5:05 AM
When I configure one module to listen on a port I can then connect to it via PC client and enter data mode. At this point a link is established and communications are asynchronous bidirectional.
When configuring one module to listen (same as above) and another to connect to a port (AT+S.SOCKON=<ip>,<port>,u), the connection can be made but data mode (AT+S) cannot be enabled on either device and communications are not bidirectional like it was talking to pc. Am I missing something obvious here? Whats the difference between talking UDP to a PC client or the module client?2016-01-29 5:48 AM
Hi Jason,
CommandMode/DataMode exists only on socket server (SOCKD). Socket client are always in CommandMode.Check ''Data Mode'' on forum main page. There are a lot of threads on how to use CM/DM.Regardsj2016-01-29 11:42 AM
2016-01-29 11:46 AM
Which FW version are you using? I don't expect hardfaults using latest version.
Please update. Contact your local distributor.Thanksj2016-02-01 7:39 AM
V3.4
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.