2023-08-23 1:42 AM
Hello st community,
I'm trying to use the BlueNRG-355 in deepstop mode with timer, to wake it up with an I/O. I used function from Power Save Modes project from the Navigator with Bluetooth function.
while(1)
{
ModulesTick();
APP_Tick();
HAL_PWR_MNGR_Request(POWER_SAVE_LEVEL_STOP_TIMER...);
}
Modulestick function is as follows
while(1)
{
ModulesTick();
APP_Tick();
HAL_PWR_MNGR_Request(POWER_SAVE_LEVEL_STOP_TIMER...);
}
However, when you enter deep sleep mode, you continue to wake up immediately for some reason.
After debugging through the HAL_PWR_MNGR_Request function, we found that we could not enter the next if statement. Is there a solution?
/* BLE Stack allows to enable the power save */ if (BLE_STACK_SleepCheck() != POWER_SAVE_LEVEL_RUNNING)
2023-12-05 10:32 AM
Hello @akkkkkk
Have you made any progress ?
I'm stuck on the same problem : bluenrg-lp-power-save-level-stop-mode-using-ble-stack
for the immediate wakeup : bluenrg2-ble-timeout
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.