Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

P-L496G-CELL02

What eSIM has been used in this P-L496G-CELL02 EVK?The B-L462E-CELL EVK is using ST4SIM-200M in the board. Would like to know the differences between the boards.Thanks.

STLearner by Associate III
  • 1439 Views
  • 1 replies
  • 0 kudos

ST Link V2 programming BlueNRG-1 inconvenient.

Hello friend,I programmed a blueNRG-1 MCU using ST Link V2. But I need to use BlueNRG-1 ST -Link Utility's application to erase MCU and need to pull up a pin (for SWD program). Then unplug the ST link V2 and plug it in. Release the pull-up pin and us...

TWu.6 by Associate II
  • 1495 Views
  • 1 replies
  • 0 kudos

Hello, I'm doing interference tests with wifi and BlueNRG-LP Prop. Is there a value how much higher the signal of the BlueNRG-LP has to be to overpower Wifi? Regards

WiFi uses significantly higher output power. I assume that the WiFi signal is perceived as noise by the BlueNRG. (Please correct me if I am wrong.) To receive a signal from a second BlueNRG-LP, the received msg signal strength must be higher than the...

Thomas1s by Associate II
  • 715 Views
  • 0 replies
  • 0 kudos

I tried to replicate the usb part of NUCLEO-F439ZI dev board to a project, without success.

I'm using vbus to power supply the MCU, through a voltage regulator. For the MCU I'm using the stm32f427, not the 39, as in the development board, but they seemed compatible with my project features.When I connect the board to my laptop via USB, the ...

0693W00000Y935rQAB.png 0693W00000Y936QQAR.png 0693W00000Y936uQAB.png 0693W00000Y93ASQAZ.png

ST7580 - AC communication

Hi,How would one implement PLC together with a combination of NUCLEO-PLM01A1 and STEVAL-XPLM01CPL?how would i need to hook up the circuitry between those two boards, so I can safely communicate over AC lines.Best regardsRené

RPoul.2 by Associate
  • 725 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.