2023-03-02 6:31 PM
What eSIM has been used in this P-L496G-CELL02 EVK?
The B-L462E-CELL EVK is using ST4SIM-200M in the board.
Would like to know the differences between the boards.
Thanks.
2023-03-03 9:34 AM
Hello,
On P-L496G-CELL02 it is no more possible to use the eSIM (validity expired).
A plastic SIM inserted in SIM socket on the modem board must be used.
However the eSIM is a ST4SIM-110M
Note it has a single profile and so does not support Remote SIM Provisioning.
ST4SIM-200M on B-L462E-CELL1 supports RSP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.