2023-03-06 12:27 AM
Hi,
I'm using BlueNRG- M2SP module & I have downloaded BlurNRG M2SA example code. In the application manual, it is mentioned that some data need to be changed like "HS_SPEED_XTAL", "LS_SOURCE" & "SMPS_INDUCTOR" while porting an existing project from BlueNRG M2SA to M2SP module and I have changed that. But only the UART peripheral program worked properly rather than that of BLE examples. GPIO toggling example is also not working, pins are not changing their states. I want to know whether there should be any extra changes required or not in M2SP module.
Thank You...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.