Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-FKI433V2 not working

Hi, I have an STEVAL-FKI433V2  board which I am trying to work on using S2-LP DK on windows.When I connect the board and try to open the com port, it requests to update the firmware on the L0.Did that, and still it does not work. It always requests t...

No "accept" button on ST BLE Sensor app

Config :Iphone 6siOS 14.8.1The user can't accept the license agreement as there is not "accept" button. user is locked on License Agreement page of the application.Work for others versions of iOS, but not 14.8.1.Also work on Android.Please patch this...

Okta Service with angular

I am using Okta  signin widget, I got user info. But I am unable to getting the specific user groups data(user belonging to which group) with okta login with angular. 

ursyathi by Associate
  • 1812 Views
  • 1 replies
  • 0 kudos

Unable to flash Bluenrg345 via Uart bootloader

Hi, this is regarding the bluenrg345 device We have developed a custom board for reading and sharing data via bluenrg deviceFor flashing we use RF flasher utility tool and uart bootloader via usb to uart icWe have flashed a couple of times using this...

Resolved! ST60A3H1 underwater performance?

The ST60A3H1 looks very interesting. While I understand an NDA is required for access to the complete details on this solution, would it be possible to say if it works underwater as communication between ROV modules?Scenario:IC A | 1mm air or mineral...

StefanH by Associate III
  • 1628 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.