2024-02-16 3:44 AM
Hi, this is regarding the bluenrg345 device
We have developed a custom board for reading and sharing data via bluenrg device
For flashing we use RF flasher utility tool and uart bootloader via usb to uart ic
We have flashed a couple of times using this method, but few of the boards (5/10) do not gets flashed
stating error as " Exit flashBoard: Exception ID1: auto baudrate functionality failed " on RF flasher tool
- we have tried couple of debugging and replaced few discrete components
- replaced bluenrg device as well
- can we know what is leading to this issue?
- What is issue and how can we solve it ?
Although flashing using STLINK and RF flasher tool for the exact same board does works
2024-02-28 4:19 AM
Hello,
For entering bootloader have you respected below sequence:
- Set PA10 to high
- Perform a HW reset
- release PA10
Then you should be able to access UART bootloader through dedicated UART PA8/PA10.
Regards
Laurent
2024-03-05 4:24 AM
Thanks for the Input ,
Yes I am following above mentioned procedure
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.