Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with reading MPU-6500 by STM32

Hi!I have a problem with reading data from MPU-6500 gyroscope/accelerometer (Arduino-module GY-6500/GY-9250). I am using the I2C protocol. When reading the WHO_AM_I_REG register ( with address = 0x75 ) I always get the number 0x70, although all publi...

How integrate my own touch driver with TouchGFX

Hi everyone!I'm trying to integrate my own touch controller with TouchGFX on a custom board. My touch driver gives me XY coordinates of an event (press or release). Basically with this information I can do whaterver I want. So, for example, I can cha...

nikof by Associate II
  • 1582 Views
  • 1 replies
  • 0 kudos

RTC: Oscillator Fail detection.

Hi All,I am currently using your RTC: M41T81M6F and I am evaluating to add, as additional homologation, your RTC: M41T81SM6F.I have seen that the “new” one has additional features such as oscillator Fail detection and Battery Low detection, however o...

AKhar.4 by Associate
  • 1186 Views
  • 0 replies
  • 0 kudos

STEVAL-FKI915V1 s2-lp

hidoes anybody nows how the auto fequency offset works?is there a register? it works only with the steval board ?how does the board calculate the correction?Thank'smarco

0690X00000ArrqzQAB.jpg
Mmila.9 by Associate II
  • 1611 Views
  • 2 replies
  • 0 kudos

Resolved! PCB design problem with Bluenrg-332ac

Hi everyone,I am currently designing my own PCB board using the bluenrg-332ac chip. I want to use the ufl/SMA port to connect my antenna without connecting the PCB antenna. So I wonder how to remove the PCB antenna from the PCB layout with only UFL p...

JasonYang_0-1709007391635.png
JasonYang by Associate II
  • 3410 Views
  • 5 replies
  • 3 kudos

STUSB1600A and STANDBY_POWER_MODE_DISABLE

Hello,The STUSB1600A has a standby power mode that is described in the datasheet as being disabled by default, and can only being enabled through NVM reprogramming.However, when using the STUSB GUI (v. 3.2.3) connected to a STUSB1600A and NUCLEO-F072...

E4A by Associate
  • 1193 Views
  • 0 replies
  • 0 kudos

Something wrong with BLENRG-MS and STM32CubeExpansion_BLE1_4.2.0 sdk, program will trap in infinite loop at SPI_IRQ.

I use BLENRG-MS and stm32l07 mcu. Mcu call the APIs to control the BLENRG-MS module. MCU initialize the ble module and start observer process by calling API,and the process will be terminated in three seconds. The problem is that program may trap in...

nfei by Associate II
  • 7750 Views
  • 14 replies
  • 1 kudos

STEVAL-IDB008V1M MacOS

Hi everyone,I recently got the STEVAL-IDB008V1M dev board, I am using a M1 Macbook Air. I tried to get Wise-Studio working but the application installs but does not open for me (yes I do have GNU make, and JRE installed).So I decided to then install ...

AOdonde by Associate
  • 1740 Views
  • 0 replies
  • 0 kudos

STEVAL-IDP004V2

I am interested in activating your sensors, STEVAL-IDP003V1, using a different IO-Link master instead of the ST master board. I have two questions: I am interested in activating your sensors, STEVAL-IDP003V1, using a different IO-Link master (Balluff...

TheWho24 by Associate
  • 1224 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.