Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SP1ML packet

Posted on April 05, 2016 at 18:13I need to send complete (and receive) custom packet through the module SP1ML to cummunicate with another SPIRIT1 board (protocol is fixed). This protocol is based on ''Basic Packet'' (no StAck nor Wmbus) with : 12 by...

HTTP timeout

Posted on April 04, 2016 at 10:58When I load a webpage from  this module with some images (not so big and non so many) the module became slow and often kill the connection (timeout). I suppose this behavior came from the limited amount of RAM, as ev...

stefano23 by Associate II
  • 1476 Views
  • 2 replies
  • 0 kudos

SPGRF crytal tolerance

Posted on April 04, 2016 at 09:50Dear Madam, Sir,Would You inform me about the type of crystal what SPSGRF board uses.I have developed and manufactured 250pcs Spirit1 boards with this crystals.http://www.ndk.com/images/products/catalog/c_NX3225GA-ST...

szabo by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

MQTT subscribe with SPMW01SA

Posted on March 31, 2016 at 08:23Hi All,For my project i am using SPMW01SA WiFi module with STEVAL-IDI004v2 evaluation board.I am trying to port MQTT client application on this and socket creation, connection and publish is working.But subscribe opt...

SPWF01 - unique IDs for SSI <!--#input--> tags

Posted on March 30, 2016 at 22:45Hi, Is there any way of assigning a unique ID to a &sharpinput tag in html, so that when I get the WIND:56: message prompting for data input, I dont have to worry about figuring out which page has been served? At th...

jamie23 by Associate II
  • 1706 Views
  • 3 replies
  • 0 kudos

WIND:11:Initial SPI read failed

Posted on March 31, 2016 at 00:04I just fired up the SPWF01S module on a prototype board that I made.  Got WIND:1, WIND:13, WIND:3, WIND:0, then this error over and over. I didn't send anything to the module.  Did I forget to connect something, is...

dworkman by Associate
  • 1051 Views
  • 3 replies
  • 0 kudos

Firmware update issue

Posted on March 30, 2016 at 10:48Good morning,  I have some problems regarding firmware update. When  I try to update firmware via serial link, I obtain this message:''Error sending message 0x31 to device'' as show also in the image: Someone can hel...

0690X00000603OeQAI.jpg
stefano23 by Associate II
  • 1488 Views
  • 5 replies
  • 0 kudos

SPBTLE-RF BLE Module (BlueNRG-MS) makes the Microcontroller to reset just after setting it in discoverable mode.

Posted on March 30, 2016 at 12:47Hello, I am using SPBTLE-RF BLE Module along with X-CUBE-BLE1 sensor demo code. The program worked successfully when run on STM32L053 Nucleo board with SPBTLR-RF module. But when we ran the X-CUBE-BLE1 code on our PC...

salman2 by Associate II
  • 665 Views
  • 0 replies
  • 0 kudos

looking for code example for connection WIFI

Posted on March 28, 2016 at 21:47Hi everyone, im using a STM32F0 Discovery Board to connect a Waveshare WIFI Modul and need some example code or some tutorials how to connect WIFI and to send/receive data & AT Commands using UART. Unfortunately i ca...

quang-vu by Associate II
  • 848 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.