2016-03-30 3:04 PM
I just fired up the SPWF01S module on a prototype board that I made.
Got WIND:1, WIND:13, WIND:3, WIND:0, then this error over and over. I didn't send anything to the module. Did I forget to connect something, is the module requiring setup, or is the module damaged? Thanks #initial-spi-read-failed2016-03-30 11:11 PM
Hi David,
a timeout value was increased inside current FW3.5. That error should not be observed anymore (if module is sane...)Which FW version are you using?BRj2016-03-31 6:19 AM
I get this at powerup:
WIND:1:Poweron (141106-0950875-SPWF01S) Which number in there is FW version?2016-03-31 6:24 AM
It's FW3.3.
November 2014We’re moving the ST Community to a new platform to give you a better and more reliable community experience.