2016-06-28 7:25 AM
I am trying to connect my SPWF01S to an AP but am not able to do so. This is the WINDS i get:
+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:74:EA:3A:D3:C4:D4+WIND:25:WiFi Association with 'InOutDemo' successful+WIND:40:WiFi Deauthentication:2+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:74:Rejected found Network+WIND:74:Rejected found Network+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:74:Rejected found NetworkAnd this is the config:# Dumping All Configuration Keys:# nv_manuf = ST# nv_model = SPWF01S# nv_serial = value# nv_wifi_macaddr = 00:80:E1:B8:33:20# etf_mode = 0# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 115200# console1_hwfc = 0# console1_enabled = 1# console1_delimiter = 0x0000002C# console1_errs = 1# sleep_enabled = 0# standby_enabled = 0# standby_time = 10# wifi_tx_msdu_lifetime = 0# wifi_rx_msdu_lifetime = 0# wifi_operational_mode = 0x00000011# wifi_beacon_wakeup = 1# wifi_beacon_interval = 100# wifi_listen_interval = 0# wifi_rts_threshold = 3000# wifi_ssid = 49:6E:4F:75:74:44:65:6D:6F:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_ssid_len = 9# wifi_txfail_thresh = 5# wifi_ht_mode = 0# wifi_channelnum = 6# wifi_opr_rate_mask = 0x00003FCF# wifi_bas_rate_mask = 0x0000000F# wifi_mode = 1# wifi_region = 1# wifi_auth_type = 0# wifi_atim_window = 0# wifi_powersave = 0# wifi_tx_power = 18# wifi_rssi_thresh = 0# wifi_rssi_hyst = 0# wifi_ap_idle_timeout = 120# wifi_beacon_loss_thresh = 10# wifi_priv_mode = 2# wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_key_lens = 00:00:00:00# wifi_wep_default_key = 0# wifi_wpa_psk_raw = 5D:50:2E:22:88:13:4B:65:CE:8A:03:E2:CF:4E:8C:64:20:69:34:83:6B:F3:0D:C2:92:1B:15:C5:0A:22:87:6E# wifi_wpa_psk_text = inoutserverdemo# ip_use_dhcp = 1# ip_use_httpd = 1# ip_mtu = 1500# ip_hostname = iwm-B8-33-20# ip_apdomainname = captiveportal.net# ip_apredirect = firstset.html# ip_ipaddr = 192.168.0.50# ip_netmask = 255.255.255.0# ip_gw = 192.168.0.1# ip_dns = 192.168.0.1# ip_http_get_recv_timeout = 3000# ip_wait_timeout = 12000# ip_dhcp_timeout = 20# ip_sockd_timeout = 250# ip_dhcp_lease_time = 120# ip_dns_mode = 0# ip_use_cgis = 0x0000000F# ip_use_ssis = 0x0000000F# ip_use_decoder = 0x000000002016-07-04 2:18 AM
Can you also share AP details? b/g/n, authentication type, PSK, etc...
Deauthentication reason 2 means:Code-2
prior authentication is not valid Regardsjerry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.