2016-06-01 7:45 AM
Hello,
I tried to delete the characteristics and the service that I created but I didn't succeed. I used the commands aci_gatt_del_char and aci_gatt_del_service but it didn't work. If I understand, I have to give the handlers of the service and/or characteristics as parameters, so I tried to delete them directly after creating them when aci_gatt_add_serv and aci_gatt_add_char give me the handlers. It always answer me 0xFF (timeout). I tried to reset the component before, I tried to delete them at the beginning of the initialization (before creating the service/characteristics) but it's always the same result. Apart of this, I managed to communicate with the BlueNRG. Any help or suggestions would be appreciated. Regards Nicolas2016-06-30 3:13 AM
Dear customer,
in attach you can find a script that explain how to perform service and characteristic deletion. I have used a BlueNRG-MS with fw stack version 7.1. To run script using the GUI, please, rename txt file as py file. Let me know if you are able to do this. Regards, Graziella ________________ Attachments : delete_service_and_char.csv : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Ht2I&d=%2Fa%2F0X0000000aJ8%2FZOtoH.b3t5Xfbpg4Cd3Y9UwtHq.lxAWFJGRraC6fC.w&asPdf=falsedelete_service_and_char.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Ht2N&d=%2Fa%2F0X0000000aJ9%2F4mYMZqLjWjnnTw2QonUFdNeGmKZBT7NMVcp04kKgSNs&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.