2016-07-04 4:15 AM
Hello Regarding BOM values of:
http://www.st.com/content/ccc/resource/technical/document/bill_of_materials/d7/c0/bb/6b/fd/17/42/16/x-nucleo-idb04a1_bom.pdf/files/x-nucleo-idb04a1_bom.pdf/jcr:content/translations/en.x-nucleo-idb04a1_bom.pdfL4, the required value is 1.8pF however the part number GRM1555C1H180JZ01 indicates 18pF, which is correct?C25, the required value is 1.2pF however the part number GRM1555C1H120JZ01 indicates 12pF, which is correct?Thanks in advance.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.