Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG 2 Bluetooth 5 APIs

Posted on April 04, 2018 at 15:30Hello, I am currently developing a BLE product using BlueNRG2. I see in the datasheet that it is Bluetooth v5 compliant, but in the sample codes for STEVAL-IDB008V1, the APIs do not support Bluetooth v5 features such...

Resolved! SPWF04Sx - STA - Scan Complete:00

Posted on April 04, 2018 at 11:59hi,wifi module SPWF04Sx is configured to STA mode and try to connect to ssid.when ssid is off, wifi module runs (without received cmd AT) and scan:+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete:00is it possible to...

Resolved! SPWF04Sx - FWUPDATE

Posted on April 04, 2018 at 12:15hi,i use AT cmd FWUPDATE to update firmware of wifi module.i see sequence in HandsOn_Draftv3.0AT+S.FWUPDATE=e,192.168.xnextAT+S.RESET -> (Soft_Reset())nextAT+S.FCFGthe FWUPDATE works well (next Soft_Reset()) but i ne...

BlueNRG-MS IRQ

Posted on December 20, 2017 at 10:37 hi. im running a provided example of HID periphProfiles. using STEVAL-IDB005V1D on NXP platform (FRDM-KL43) SPI lines are OK, i can read header from the blueNRG-MS. the thing is IRQ always high. so that ...

asafbit by Associate II
  • 4829 Views
  • 10 replies
  • 0 kudos

SPWF04: Need a pull down at RTS

Posted on March 02, 2018 at 16:34Hi,I changed on my hardware the SPWF01 against a SPWF04 module. I communicate with the module via a STM32. If I use the SPWF04 module, I need a pull down resistor at the SPWF RTS output to get the communication worki...

SPIRIT1 not entering into LOCK state

Posted on April 04, 2018 at 07:02Hi,First of all, sorry for the lengthy message.We are developing a 433 MHz transceiver using SPIRIT1. We were able to run 'SDK_BasicGenreic_A' program provided with the development kit on 'STEVAL-IKR002V3D' daughter-...

SPIRIT1 not entering into LCK

Posted on April 04, 2018 at 06:56Hi,First of all, sorry for the lengthy message.We are developing a 433 MHz transceiver using SPIRIT1. We were able to run 'SDK_BasicGenreic_A' program provided with the development kit on 'STEVAL-IKR002V3D' daughter-...

SPWF04SA datasheet clarifications

Posted on April 03, 2018 at 18:43Hi ST team,Looking over the device datasheet, I had expected to see maximum current consumption at least under TX and RX conditions so I can design power management appropriately.  When this information is missing, I...

SPWF04 File print Not Responding

Posted on March 28, 2018 at 17:00I have been able to use the File Print (AT+S.FSP) in some test situations, but now that I'm using it for real I'm not getting any results.When I was performing my feasibility tests I was printing sections from within...

Resolved! SPWF01SA custom HTTP POST request Problem!

Posted on March 15, 2018 at 07:44Hello and good day!I'm attempting to use the SPWF01SA module with an STM32F0 microcontroller to post some data onto a remote web server. I have come to understand that the  AT+S.HTTPPOST command can only post form da...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.