2018-04-04 2:59 AM
hi,
wifi module SPWF04Sx is configured to STA mode and try to connect to ssid.
when ssid is off, wifi module runs (without received cmd AT) and scan:
+WIND:21:WiFi Scanning
+WIND:35:WiFi Scan Complete:00is it possible to stop/manage Wifi scanning?
WiFi Scanning is it link to a setup variable? (wifi_region, ip_allow_port_scans)
is it possible to give more details about scan?
thks
Yoann
Solved! Go to Solution.
2018-04-04 5:52 AM
Hello Yoann,
when the SPWF04 is configured as STA, it performs a periodic scan to look for the configured SSID. If that SSID is not found or suddenly disappear then the SPWF04 will keep scanning until the SSID is found again and all network features are still available.
The periodic scan can be disabled by shutting down the wifi stack (AT+S.WIFI=0) or by setting the SPWF04 in Idle mode (wifi_mode=0). However, some network operations (like AT+S.SCAN) are available when the SPWF04 is in Idle mode, whereas all network features are disabled after AT+S.WIFI=0.
Regards,
Elio
2018-04-04 5:52 AM
Hello Yoann,
when the SPWF04 is configured as STA, it performs a periodic scan to look for the configured SSID. If that SSID is not found or suddenly disappear then the SPWF04 will keep scanning until the SSID is found again and all network features are still available.
The periodic scan can be disabled by shutting down the wifi stack (AT+S.WIFI=0) or by setting the SPWF04 in Idle mode (wifi_mode=0). However, some network operations (like AT+S.SCAN) are available when the SPWF04 is in Idle mode, whereas all network features are disabled after AT+S.WIFI=0.
Regards,
Elio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.