2018-04-04 3:15 AM
hi,
i use AT cmd FWUPDATE to update firmware of wifi module.
i see sequence in HandsOn_Draftv3.0
AT+S.FWUPDATE=e,192.168.x
next
AT+S.RESET -> (Soft_Reset())
next
AT+S.FCFG
the FWUPDATE works well (next Soft_Reset()) but i need to restart (power off/on) wifi module.
is it correct?
what is the good practice after the FWUPDATE? (same with FSUPDATE)
thks
Yoann
Solved! Go to Solution.
2018-04-04 5:30 AM
Hello Yoann,
the FW update is performed at boot, so after calling AT+S.FWUPDATE you must perform a (sw or hw) reset or a power off/on cycle. Please take care that the SW reset (i.e. reset by AT+S.RESET command) drives the reset line to low level for the time necessary to reset the SPWF's micro.
Once the FW update has been completed an HW reset is raised by the module itself and the SPWF04 restarts with the new FW. If something goes wrong during the update (e.g. corrupted or wrong FW, wrong AES key,), then the 'new FW' is erased from flash and the SPWF04 is restarted with the last FW.
Might it be the case that the reset line is tight high by the host controller?
Regards,
Elio
2018-04-04 5:30 AM
Hello Yoann,
the FW update is performed at boot, so after calling AT+S.FWUPDATE you must perform a (sw or hw) reset or a power off/on cycle. Please take care that the SW reset (i.e. reset by AT+S.RESET command) drives the reset line to low level for the time necessary to reset the SPWF's micro.
Once the FW update has been completed an HW reset is raised by the module itself and the SPWF04 restarts with the new FW. If something goes wrong during the update (e.g. corrupted or wrong FW, wrong AES key,), then the 'new FW' is erased from flash and the SPWF04 is restarted with the last FW.
Might it be the case that the reset line is tight high by the host controller?
Regards,
Elio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.