Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP Sigfox registration

Posted on May 09, 2018 at 22:22Hello,during my S2-LP Sigfox registrator process, I've sent the generated e-mail to mailto:sigfox@st.com. But the response contained an error:Error while responding to [...].Error Code: 2Message: No more ID in the data...

USB-C with STUSB4500 - get power from laptop

Hello :)This USB-C is confusing me. According the standard you should be able to receive or to send power. I am using the STEVAL-ISC005V1 Eval board form ST. Unfortunately the PD2 and the PD3 line is not active if I plug the device into a Laptop.So m...

hcls by Associate II
  • 1135 Views
  • 2 replies
  • 0 kudos

Wwhen I have the user code in place, if I connect to it or disconnect from it (depending on what user code is in there), it goes into a HardFault exception if the phone touches it.

Environment: Usingng the SPBTLE-1S "postage stamp" on my own board [3v3 supply, external regulator from 12-400V, 100mA available], (using the programming/serial from a STM32F030 Nucleo board) and that works quite well (wish it supported more break...

PGigl by Associate II
  • 583 Views
  • 0 replies
  • 0 kudos

Resolved! Products: Two PCBs Steval-FKI433V2 and S2-LP DK_1.2.1 project example "SDK_Chat.c". How correctly organize echo of Rx data in one of the Steval without connecting it to terminal?

Hello.I use the S2-LP DK_1.2.1 project example "SDK_Chat.c" as the base for two Steval-FKI433V2 PCBs.The 1st Steval with unchanged SDK_Chat.c program is used as a base device, connected to COM-port, the 2nd Steval without connection to COM-port shoul...

bvn123 by Associate II
  • 2750 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.