2019-03-27 4:10 AM
I'm working with the STEVAL-IDB006V1 Board. I want to see the Bluetooth MAC address of "smartphones". I can see the MAC address of other BLE development boards, but I can't see the MAC addresses (or device name) of "smartphones" as a result of the scan. Is something like this possible with this board. How can I do it?
2019-03-27 11:35 PM
Hello,
Looks like the question is generic and not specific to BLE-Mesh
Kindly clarify which firmware you are running ?
Can you use any available project to see if the board is working fine ?
Thanks
2019-03-28 1:45 AM
Hello,
I did settings from the BlueNRG GUI program (firmware: BlueNRG_VCOM_1_8.hex) and did active scanning, not found the MAC addresses of smartphones. When I edited a BLE / IAR project and found the MAC addresses of other development cards, I couldn't see the smartphones.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.