2019-03-26 9:57 PM
my project is based on energy optimization of stm32f303. so for that how i supply different input voltage (because i use dynamic voltage scaling) and i how i measure the current value?
2019-03-27 12:10 AM
Download the F30x DSP Peripheral Library from ST's site, which contains a FFT example.
This example progam uses a constant data array as input. Replace this constant array with your own data, which you get from the ADC.
Said peripheral library also contains ADC examples you can use for a start. They will need some tweaking, because the ADC channel might not match, and the generally used ADC mode (continuous mode) is not appropriate for Fourier analysis.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.