Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP and mesh stack

Hello,Is s2-lp RF module supports mesh? If yes, where can'i found mesh stack and how it can be used?​Is below application note describe how can'i configure s2-lp module to work on mesh network? https://my.st.com/resource/en/design_tip/dm00567382.pdf​...

BMoha.19 by Associate II
  • 2364 Views
  • 6 replies
  • 0 kudos

X-NUCLEO-IDB05A1 CODE EXAMPLE NOT WORKING

Hi, I have recently buy an X-NUCLEO-IDB05A1 in combination with a NUCLEO-L053R8. The documentation furnished with those board says that there is working code examples in form of a .bin file that you just need to drag and drop in the NODE_L053R8 "driv...

MBrau.16 by Associate
  • 759 Views
  • 0 replies
  • 0 kudos

Why do i not get disconnection complete event if i want to disconnect from paired bluenrg-ms with my smartphone?

I managed to pair bluenrg-ms with my smartphone. (pairing complete arrives with status = 0x00 and everything is okey) but if i want to disconnect from it i can't get any events. I can press "disconnect from paired device" on my phone but nothing hap...

Not able to program STEVAL-BLUEMIC-1

I am using STEVAL-BLUEMIC-1. which is having firmware already(Accelerometer ,Gyroscope and Voice) with BLE. I want to load new firmware in that. But not able to load through ST LINK . Read out protection enable is coming. I try to disable the read ou...

mikt by Associate II
  • 1252 Views
  • 2 replies
  • 0 kudos

STEVAL-FKI 001 V1

Development board "STEVAL-FKI 001 V1" has been obtained.But I used a simple microcontroller like Arduino.So, "STEVAL-FKI 001 V1"Which language to developI do not know where to download the development environment.I want you to help me.

WYusa by Associate
  • 937 Views
  • 1 replies
  • 0 kudos

[SPSGRFC] Help configuration

Hi to all.I'm working on telemetry board:P2P, client connects to a server (microcontroller) just for request, then server starts to send every second data to client (up to 10'000 Bytes), so I need to work at least at 115200 bit/s (actually I'm using ...

mbertoni by Associate II
  • 1139 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.