Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi ST I am trying to working on gpio interrupt on my BlueNRG-1 and am using the Dio 13 which is meant for and also know was INT1 pin I see that the interrupt is being triggering only on the rising edge but not the falling edge can u please help

Also I am trying to use dio9 which has internal pull up ..for triggering the interrupt it seems to not detect both rising and falling edge in this case Can u please help ​

Anikh.1 by Associate
  • 1033 Views
  • 0 replies
  • 0 kudos

how to use demo codes

I'm very first time using bluenrg1. I saw a lot of sample codes. In my project I have to use two i2c one is to receive data other is to display data.also I want to send the data through bluetooth. For these cases which demo code is suitable. please h...

RJOY.1 by Associate III
  • 1091 Views
  • 0 replies
  • 0 kudos

Resolved! Question about BlueNRG-2 radio driver

Hello,I would like to develop a sniffer using BlueNRG-2 chip. Each system will be able to transmit packets with an unique ID and to receive packets from the other devices nearby (also devices based using BlueNRG-2). The aim is that all the devices sh...

Stabilo by Associate III
  • 1482 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.