2020-04-02 6:48 AM
Hello,
I would like to develop a sniffer using BlueNRG-2 chip. Each system will be able to transmit packets with an unique ID and to receive packets from the other devices nearby (also devices based using BlueNRG-2).
The aim is that all the devices should be able to estimate how many devices are nearby.
For that, I would like to use the radio driver directly. I think using BLE will only add some complexity. What do you think ?
But I am a bit confused about the "Network ID". Is it possible to have, let's say 10 devices close by, and communicating on the same Network ID ?
Thanks a lot!
Solved! Go to Solution.
2020-04-08 9:55 PM
> Is it possible to have, let's say 10 devices close by, and communicating on the same Network ID ?
Yes. Just configure these devices same Network ID and communicate on the same channel.
2020-04-03 10:55 PM
you can find Radio driver in STSW-BLUENRG1-DK
2020-04-08 9:55 PM
> Is it possible to have, let's say 10 devices close by, and communicating on the same Network ID ?
Yes. Just configure these devices same Network ID and communicate on the same channel.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.