Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Teseo-LIV3F - a big bang for the buck ?

Off-the-shelf GNSS receiver modules like new Teseo-LIV3F makes sense for application developers without any advanced software requirements and without too much RF expertise. In this case people can achieve fast results and avoid hassle compared to a ...

Kersten by Associate II
  • 1255 Views
  • 1 replies
  • 0 kudos

Enabling notification for BlueNRG1 characteristics

Hello,I am using the BlueNRG 1 stack ​V2.5.0.I am using the callaci_gatt_add_char(SeviceHandle, UUID_TYPE_128, &char_uuid, 20, CHAR_PROP_READ | CHAR_PROP_NOTIFY, ATTR_PERMISSION_NONE, 0, 7, 1, &CharHandle);But I am seeing that I don't always see the ...

TSane.1 by Associate II
  • 840 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L476VGT UART4 with GSM module SIM7000E

Hello,I'm trying to connect SIM7000E with STM32L476VGT by using UART4 (PA0 as Tx and PA1 as Rx)I'm already using USART2 to show messages in RealTerm and I can't use the other UARTs because I can't find the pins on the board.This is the code I'm tryin...

Moughit by Associate III
  • 2604 Views
  • 5 replies
  • 0 kudos

Resolved! BlueNRG-2 repeatedly sending IRQ requests on boot.

Hello, I have configured a BlueNRG-M2SA as a network coprocessor using the provided DTM_SPI.hex file. I have connected it to an external uC and am able to read data from it. The problem is that as soon as the BlueNRG boots up and the interrupt is ena...

JTorr.1 by Associate II
  • 1354 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.