Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Could you advise us whether CMOS camera has electrical saturation in switched off mode due to flashlight exposure right before dim fluorescence signal acquisition?

I am a researcher from Macquarie University. We're interested in using your CMOS cameras in-built in a smartphone for research and business purposes. We're trying to detect fluorescent signal in millisecond time frame right after a flashlight.Looking...

NLipe.1 by Associate
  • 991 Views
  • 0 replies
  • 0 kudos

Run BlueNRG-MS with BlueNRG GUI and STLINK-V3SET

Hello,I bought an STEVAL-IDB005V1D board with an BlueNRG-MS chip. Is it possible to control the chip with BlueNRG GUI through the SPI of the STLINK-V3SET ?I could do it for a BlueNRG-M2 board through UART, but it does not seem to work with the BlueNR...

VGros.3 by Associate III
  • 747 Views
  • 0 replies
  • 0 kudos

Setting up STUSB4500 sink for 12V,5 A

We are using the STUSB4500 PD chip in one of our applications. The requirement is to set the Power delivery to 12 V and 5A for the sink. I have been referring the driver code provided by ST to program our microcontroller. To set PDO to 12 V and 5 A, ...

ARadh.1 by Associate III
  • 7746 Views
  • 18 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.