2021-02-18 3:42 PM
Hi,
There are three type of source PDOs:
Documents gave examples for the decision algorithm for Fixed Supply type source PDOs. But for Variable Supply (non-Battery) and Battery type of source PDOs, the voltage is a range rather than a single fix number. So a match happens when required voltage fall into the range and the required current is less than or equal to the source Operational Current (for Variable Supply(non-battery) type), and the required power is less than or equal to source Operational Power(For Battery type), right?
Thanks,
Yan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.