2025-07-29 9:36 PM
Hi,
I would like to use an external signal to trigger camera capture with the STEVAL-EVK-U0I board. I am using a promodule (CAM-56G3), and looking at the document: how-to-integrate-and-configure-the-vd56g3-vd66gy-and-vd16gz-devices (p.g. 22 section 1.3), I know it should be possible to do this by using the gpio 0 pin, and setting the first 2 bits of the VT_CTRL register to EXTERNAL_SYNC. However, it is unclear to me if the STEVAL-EVK-U0I board exposes the gpio pin I need or if there is another way to go about this with the STEVAL-EVK-U0I board and a promodule.
Thanks
Solved! Go to Solution.
2025-07-30 1:27 AM
Hi @oaa3wf ,
The gpio 0 pin is accessible through R55. I agree that this is not easily accessible, but you should be able to connect a wire to your external trigger source.
Best regards,
Jean
2025-07-30 1:27 AM
Hi @oaa3wf ,
The gpio 0 pin is accessible through R55. I agree that this is not easily accessible, but you should be able to connect a wire to your external trigger source.
Best regards,
Jean
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.