Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L4CX Dealing cleverly with multiple object ranging

 Hi all, I'm back with another question re: our 5-TOF setup (VL53L4CX x 5, all 'looking' out of the centre of a spherical sculpture, trying to detect and interpret people approaching and interacting with it).I posted earlier about trying to multiplex...

MGG_0-1753985163280.png
MGG by Associate II
  • 766 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L0X and RP Pico W

I'm trying to port the VL53L0X library for use with the RP Pico W for academic reasons, but I can't map the calls between the VL53L0X SDK and the RP Pico W SDK. For example, the function int32_t VL53L0X_read_multi(uint8_t address, uint8_t index, uint...

Video stream from VD55g1

Hi, I have teh VD55G1 connected to UCM-IMX8m PLUS sbev from compulab Here is the links to the SBC : https://www.compulab.com/products/computer-on-modules/ucm-imx8m-plus-nxp-i-mx-8m-plus-som-system-on-module-computer/ I am compiling the driver with my...

VL52L1X with Serial on Arduino Mega

I use the VL53L1X TOF- Sensor on an Arduino Mega.With just the Sensors, everything works well.But when I try to read from Serial1 (and I tried Serial2 and 3 as well) I do not receive any Data from the SerialPort.Without the Sensors the SerialPorts wo...

Serafina by Associate
  • 478 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX sensor - GO2 error status

Hello,We have an issue with the VL53L7CX. We are using 2.8V for both IOVDD and AVDD. We have 4x TOF sensor on the same I2C line. We set the LPn for 3x of them to low to disable the i2c comm. We are only using 1x TOF for now with it's LPn set to High ...

FB__1 by Associate III
  • 696 Views
  • 3 replies
  • 0 kudos

VL53L1X Interrupt not working, No measurements

Hi, I am having trouble with the interrupt. I manange to coummunicate via I2C and read Model ID and Type. But my problem is that i can't initiate the sensor via the VL53L1X_SensorInit() function in the Ultra Lite Driver I'm using. When I debug I see ...

Resolved! Strange start-up behaviour of VL53L5CX ToF sensor

Hello Developers, Hello ST-Team,unfortunately we are stuck in implementing VL53L5CX on our PIC18. We see a strange clock stretching behaviour of the sensor and problem downloading the firmware.We implemented Ultra Lite Driver 2.0.0 in an application ...

Joh70_0-1746790956757.png Joh70_1-1746791711071.png Joh70_0-1746793224931.png Joh70_2-1746791875643.png
Joh70 by Associate II
  • 2158 Views
  • 5 replies
  • 0 kudos