Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

about argument of VL53L1X_CalibrateXtalk()

Dear Sir,There is a question about argument  VL53L1X_CalibrateXtalk().For cross talk calibration, we will use  VL53L1X_CalibrateXtalk()  with argument of uint16_t TargetDistInMm,we should give Xtalk calibration distance to  the argument. But, we wond...

DSai.1 by Associate III
  • 1533 Views
  • 1 replies
  • 0 kudos

Resolved! Looking for a Distance calculating Sensor

Hi ,we are looking for a distance sensor that meets the below requirements1.Working distance 5mm to 200mm2. Resolution steps: 0.01mm steps what is the minimum resolution steps your sensor can provide. Let me know if you need anything else. 

Resolved! I2C address problem with SATEL-VL53L7CX

Hello everyone,I am trying to read the distance data from a VL53L7CX ToF sensor with a Teensy 4.1 board. I am using the SATEL-VL53L7CX breakout board. The sensor is detected by the Teensy, however I when I try to check if the new data are ready to be...

Resolved! VL53L5CX VL53L5CX_ResultsData distance_mm mapping

Hello,Been thru all the specs I can find on the VL53L5CX but I can't find how the Zones numbers map to array of distance_mm in the VL53L5CX_ResultsData  struct.Is Zone 0,0  distance_mm[0] please?Or can someone point me to the spec/page please?Many th...

Iknig.1 by Associate II
  • 1601 Views
  • 1 replies
  • 0 kudos

VL53L5CX Histogram Data at Low Frame Rate?

I read in other posts that it is not possible to read out the VL53L5CX histogram data because there is just too much of it. But I was wondering if it is possible to read it out if we do not care about real-time operation and are okay reading out the ...

FGuti.2 by Associate II
  • 2807 Views
  • 5 replies
  • 0 kudos

Anyone using VD6283 without stmcube ?

Hi everybody, I'm trying to interface vd6283 (I own vd6283-satel breakout board) with other non-stm32 microcontrollers (esp32, samd21, ecc) .stm's library (x-cube-als) claims that "should" be easy porting on another hw but...it's not that easy....Did...

MZ68 by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos

Is there an ACTUAL datasheet for the VD6283 available?

Having been using ST sensors for decades, this is the first time I stumble onto this perplexing problem: there is no datasheet available!There is a .pdf called 'datasheet', but it only documents half the registers and them very superficially. There i...

KPalo.2 by Associate
  • 1339 Views
  • 1 replies
  • 0 kudos