Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L8CH Drop in for VL53L8CX

I'd like to work with the raw histogram data from the VL53L8CH, which I don't believe the VL53L8CX has. Currently, I don't think that there's an evaluation board for the VL53L8CH, but it says it is "pin-to-pin" compatible with the VL53L8CX. Does this...

JGarrettW by Associate II
  • 4398 Views
  • 4 replies
  • 3 kudos

VL6180X

Hi ST experts,Is VL6180X comparable with TMD2635? 

STLearner by Associate III
  • 1109 Views
  • 1 replies
  • 0 kudos

Intrinsic matrix of VL53L8CH/X

Hi there, I have recently met a problem in calibration of VL53L8CH/X. So I need to get its intrinsic matrix. Where can I find it?

Bryce by Associate II
  • 1773 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L5CX not measuring far distances

I am using multiple VL53L5CX sensors to measure distances around a robot using the 4x4 resolution, target order closest and ranging in countinuous mode. When I'm measuring a distance close to the sensor ~500mm and then the object is suddenly removed ...

mreumer by Associate
  • 2449 Views
  • 2 replies
  • 1 kudos

water level monitor with time of flight sensor

Hi friends,  currently Iam working for the project (water level monitor with time of flight sensor).  For my application it should sense  around 4 meters.  I have selected the sensor (vl53l5cx) which is 2.7 meters sensing range which black reflective...

Arun by Associate
  • 1573 Views
  • 1 replies
  • 0 kudos

Resolved! About temperature calibration of VL53L1X

Hello,I am developing a system using VL53L1X.I have read UM2510 (A guide to using the VL53L1X ultra lite driver).This library implements the function called "StartTemperatureUpdate".The description for this function states, "This function performs th...

KArai.2 by Associate II
  • 3214 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CX long series of bad measures

Hi, I'm testing some VL53L4CX for about 10 months with nrf52832 using I2C. It's used in very dark conditions and within 3m and I take 15 measures 24 times a day.Between periods of measures I completely power off the sensor with an LDO.It works fine f...