Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VD6283 Sensing problem with range?

I have been using VD6283 with STM32 and have found that they work well in detecting flicker when the light source is near the sensor. However, I have encountered an issue where the flicker is not detected when I move away from the light source.Additi...

MKash.3 by Associate
  • 1502 Views
  • 1 replies
  • 1 kudos

VL53L4CD cover glas specification

I am using the VL53L4CD for my current project and I would like to add acrylic glas cover to it. I am actually using 4 of the ToF Sensors and would like to cover all of them with one glas.What type of glas can be used here, are there any known limits...

DrD00m by Associate III
  • 2134 Views
  • 2 replies
  • 1 kudos

VL53L4CD using characterization GUI Tool

Hi,I purchased the P-NULCEO-53L4A1 package and am testing it to use Liquid Level Monitoring.I have downloaded STSW-IMG039 and am referencing AN5851 and STSW-IMG039-L4CD.pdf.I used the provided GUI Tool (GUILiquidLevel.exe) for Nonliearity correction....

LJinH1_0-1691033942833.png LJinH1_1-1691033948232.png LJinH1_2-1691034240182.png LJinH1_3-1691034551871.png
LJinH.1 by Associate II
  • 2947 Views
  • 5 replies
  • 3 kudos

Power Cycle VL53L5CX limit

Hello,I am a committed STM32 addict and currently using the STM32F411 with nine VL53L0X's on a wheel robot project, which is working pretty well. However sometimes due to poll rate and beam angle/distance/speed small (narrow) objects are not seen unt...

Iknig.1 by Associate II
  • 1508 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX/VL53L5CX API similarity and part identification

I'm looking into using the VL53L7CX on a board designed for the VL53L5CX. I expected it to be a drop-in replacement on the hardware side with only a change in software needed (using the L7CX API instead of the L5CX API), but when I compared the two A...

kwc by Associate III
  • 3761 Views
  • 3 replies
  • 1 kudos

Resolved! VL53L5CX ULD and device power consumption

I see that the VL53L5CX sensor has two voltage supply alternatives, both for the digital part (IOVDD) and the analog part (AVDD). I am also observing that starting from version 1.3.3 of the ULD driver, we have a function called vl53l5cx_disable_in...

Resolved! VL6180X trouble picking out the best target object

Hello all,I am confused on some test results that we performed while gauging the VL6180X's performance and am seeking some advice. We are testing various materials with the intention of using the best performing one for the target object in our appli...

AGome7_0-1688075316771.png AGome7_1-1688075642344.png AGome7_2-1688076236957.png
AGome.7 by Associate II
  • 3109 Views
  • 3 replies
  • 0 kudos