Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L3 integration time

I want to know whether the calculation of integration time using kcps and signal peak count is correct or not Signal = 3.83 kcps/spad (3.83*1000*211(SPAD ea ))/2099  =385    =>  1/385 = 2.6 ms Ambient & signal kcps, is the integration time the same?...

WJLO_0-1690975033577.png
WJLO by Associate II
  • 2638 Views
  • 3 replies
  • 0 kudos

Controling INT PIN on VL53L7CX

Hi everyone!I have a not conventional question to this device. INT pin is used in library to send interrupt to MCU. In my case i use just necessary part of library so the INT pin is not used at all.So now the question. Is it possible to use it now th...

MŻbik.1 by Associate II
  • 2451 Views
  • 3 replies
  • 0 kudos

Resolved! issue during VL53L1X crosstalk calibration

Dear Sir, We are currently in the process of conducting crosstalk calibration using the VL53L1X ultra-lite driver, but unfortunately, the results we're obtaining are not as expected. Our approach involves utilizing an A4-sized gray chart board as the...

DSai.1 by Associate III
  • 3806 Views
  • 4 replies
  • 2 kudos

VL6180X -- Unexplained "Waves" in Time of Flight Data

Hi there, My team and I have noticed an irregularity in our VL6180X sensor data that we do not understand. Despite having a stationary target (~75mm away), the calculated range values from the VL6 appear to "wave" over time, and do not settle into a ...

Kurt123_0-1690835562838.png Kurt123_1-1690835613360.png
Kurt-123 by Associate II
  • 4750 Views
  • 7 replies
  • 2 kudos

Resolved! VL53L4CD - Calibration Procedure and Tools

Hello,I'm working with VL53L4CD to have the distance between the board and some liquid. This distance could go from 20mm to 250mm. We want to protect the board with a glass and then do a calibration, first Offset then Crosstalk. Into the user manual,...

GCout.1 by Associate II
  • 4123 Views
  • 3 replies
  • 0 kudos

Resolved! cover glass vl53l5cx

by using the cover glass can the sensor still able detect close ranges (after calibration)

tarlan by Associate
  • 2189 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1CB single shot fail

Hello,I'm using a VL53L1CB with X-CUBE-TOF1 but when i try to use the blocking one shot mode, i always get 0 target.If i use the blocking continuous mode, the first measure will always return 0 target and only the second measure will return a target....

nicolas by Senior II
  • 1963 Views
  • 2 replies
  • 0 kudos