Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ToF VL53L4CD load capacitance calculation

Hi, I am struggling to understand how to calculate the load capacitance when adding the pull-up resistors in my circuit with VL53L4CD ToF sensor to run the sensor in fast mode plus. The datasheet states that:Suggested pull-up and series resistors for...

Gabor23 by Associate II
  • 2297 Views
  • 3 replies
  • 0 kudos

Reading several VL53L7CX sensors with a Nucleo

Hello everyone,I am trying to read data from three SATEL-VL53L7CX, using only their mini-PCB part, with a Nucleo F401RE.To do so, I did the following wiring:each sensor is using a different I2C bus (sensor 1 is plugged on SDA1/SCL1, sensor 2 on SDA2/...

VL53L7CH, VL53L8CH with AI

As it is described both models are dedicated for  AI applications. Where can I find examples of usage or materials to start?I assume I can use NEAI Studio?

KNawa.1 by Associate II
  • 2067 Views
  • 3 replies
  • 0 kudos

VL6180X sensor initialization SR03 setting

Hi, I was wondering what is the SR03 settings in initialization of VL6180X ToF sensor? I had gone through the user manual & application note AN4545 but i couldn't get the answer. If someone knows please explain. It just for educational purpose only.T...

AK_19 by Associate
  • 2620 Views
  • 1 replies
  • 0 kudos

Resolved! Something Wrong with Calibration of VL53L3CX

Vl53l3CX works well when i init it with DataInit and StartMeasurement Function,but when i add a OffsetCalibration to its init sequence,it output a distance of 8191 mm,which is obviously wrong .Paraments of calabration function are shown in the  follo...

屏幕截图 2023-10-08 155108.png 屏幕截图 2023-10-08 154035.png 屏幕截图 2023-10-08 154127.png 屏幕截图 2023-10-08 154900.png
LOMO by Associate III
  • 1582 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L5CX offline

I purchased X-NUCLEO-53L5A1 and NUCLEO-F401RE board. I assembled them and followed the Quick start guide X-NUCLEO-53L5A1 manual. I can't connect the device in the VL53L5CX. I update firmware and ST-Link before. I connected to the ST COM port via term...

JVane.1 by Associate II
  • 8007 Views
  • 6 replies
  • 0 kudos

Resolved! VL53l0x I cannot measure more than 400mm

Dear Sir,     I am trying to read the distance from the VL53Lox i can read upto 400mm , when i try to measure more the 400mm it is not reading proper reading. Please guide 

Yusuf1 by Associate
  • 2521 Views
  • 2 replies
  • 0 kudos

Resolved! Disabling VL53L5CX Autocalibration?

Hi there!​I was wondering, for a school project, if it is possible to disable te autocalibration on the VL53L5CX and if it would be possible to manually calibrate it?​Thanks! :fox_face:

TVos.1 by Associate
  • 2328 Views
  • 3 replies
  • 0 kudos

VL53L7CX_ResultsData interleaving & format

The ULD driver VL53L7CX_ResultsData object type contains range data from the VL53L7CX.  Each member that holds data for multiple zones and targets is organized in an array.Items signal_per_spad, range_sigma_mm, distance_mm, reflectance & target_statu...