2023-07-04 3:33 AM
Hello,
I'm using a VL53L1CB with X-CUBE-TOF1 but when i try to use the blocking one shot mode, i always get 0 target.
If i use the blocking continuous mode, the first measure will always return 0 target and only the second measure will return a target.
The workaround is not ideal because it use 3 times more energy than the failing one shot (~1.8mC vs ~0.6mC).
Is there something special to do to make the one shot mode working correctly ?
Solved! Go to Solution.
2023-08-04 2:35 AM
Hello
We identified the issue and it will be fixed in the next release of the package planned for end of the year. Sorry for the delay.
Best regards
Anne
2023-08-04 2:35 AM
Hello
We identified the issue and it will be fixed in the next release of the package planned for end of the year. Sorry for the delay.
Best regards
Anne
2023-09-01 7:11 AM
Hello,
Thank you for providing me via email a fix for the X-CUBE-TOF1 3.3.0. The first measure is now working.
Best regards,
Nicolas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.