Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! vl53l5x GO2 error on 8x8 resolution

Hi,I managed to get the sensor working with firmware VL53L5CX_1.3.11. It works even if I reduce the data load and disable everything except distance.My problem is, that I do not receive any data if I switch the resolution to 8x8 - the sensor is only ...

Thomas6 by Associate II
  • 2280 Views
  • 4 replies
  • 0 kudos

How to implement the VL53L3CX on a Raspberry PI3

My goal is to implement the VL53L3CX TOF sensor on a Quanser Qdrone as a sensor for height control. As an inbetween I am trying to get the VL53L3CX working with my Raspberry PI3 first to better understand how the sensor and API work. So far I have no...

AGree.4 by Associate
  • 5815 Views
  • 7 replies
  • 1 kudos

Resolved! VL53L8CX Power consumption is too high

Hello,in the datasheet for the L8, the power consumption for a low power mode such as autonomous 4x4, 1Hz frequency and 5 ms integration time is given to be 1.6 mW . I tried measuring the power consumption for a similar mode which is autonomous 4x4 @...

simonbelanger_0-1725030402551.png simonbelanger_1-1725031416679.png

VL53L5CX _start_ranging() fails with 255 error

Hi all,For the last several days I have been battling this API for the VL53L5CX and finally reached the point where the initialisation passes every time. I proceed to set some of the configuration parameters (mostly resetting to the default values su...

0693W00000aIQYxQAO.png
ALohr.1 by Associate II
  • 14188 Views
  • 13 replies
  • 0 kudos

Resolved! VL53L0X API usage guidelines

I've tried to use VL53L0X API, but it is too confusing. The API package STSW-IMG005 lacks any proper guidelines how to use API. The source file vl53l0x_platform results in one or another error.i'm unable to my own code VL53L0X as register map is not ...

NSing.5 by Senior
  • 3841 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L7CH does not recognise the closest object

I put a object at about 1100mm, and another object at about 50mm. And use example5 to test vl53l7ch (4x4 resolution, max 2 objects per zone), but found that it does not recognise the closest object. For example, zone 13 output:[Zone13] (found 1 objec...