Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The sample code for the VL53L5A1 sensor cannot be built.

This is my first time posting.Thank you for viewing. ・I would like to use the VL53L5A1 sensor with the STM32L0 series.・Created according to the manufacturer's document "UM2974".・When I created it with STM32CubeMX Ver6.11.0, the build did not pass. Th...

NEO-MEC by Associate
  • 4041 Views
  • 2 replies
  • 0 kudos

RANGING_FREQUENCY - VL53L8A

Hi,I am testing VL53L8A with NUCLEO-F401RE and 53L8A1_SimpleRanging software under STM32CubeIDE.Changing RANGING_FREQUENCY from 5U to 15U does not increase the frame rate, always 5Hz.What am I doing wrong? I have changed also the TIMING_BUDGET to 5U ...

Resolved! VL53L8CX distance matrix

Hello,I am using a VL53L8CX sensor in 8x8 mode. There is a thing that is unclear to me from the documentation, so I need a clarification. A value in the zone Z of the matrix I get from the ToF sensor is:a) Distance between the object in the zone Z an...

milukic by Associate II
  • 1928 Views
  • 2 replies
  • 1 kudos

Resolved! VL6180X range measurement scaling

HiFrom a the VL6180 documentation i found that there is a scaling factor.As i read from it, the default is 3 and this means that the response are in mm (1mm resolution)If it is changed to 2, the result will have a resolution of 2/3 mm ect. But in the...

Resolved! VL53L3CX i2c error (can't scan address)

I'm using VL53L3CX. The development board is nucleo f103rb. Power was supplied from the laptop, and pin connections were the same as shown in the notes in the example code.(sensor - pololu / code - stm32arduino helloworld)The sensor was powered to 3....

Resolved! VL53L5CX-SATEL won't respond to I2C?

 I'm trying to get the VL53L5CX-SATEL to talk to a microcontroller.The lines are connected as followsINTFloatingI2C_RST22K pull downSDAMCU SDA Pin with 2.2K pull up to 3.3vSCLMCU SCL Pin with 2.2K pull up to 3.3vLPn22K pull up to IOVDD (3.3V)PWREN22K...

nack.png
CSkil.1 by Associate II
  • 2188 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L5CX-SATEL schematics?

Is there a publication of the detailed schematics for the VL53L5CX-SATEL? My search of the ST site returned two documents only showing high level connections. I'm more interested in which signal lines, capacitors, resistors, and values are populated...

TPhil.3 by Associate II
  • 7877 Views
  • 8 replies
  • 7 kudos

Resolved! I2C of VL53L1

HI,I am using VL53L1 sat board, can i configure I2C of the sensor to 1MHz? How should i do it? Could u please guide me on this matter?Thank you

vishnusf by Associate III
  • 2553 Views
  • 5 replies
  • 1 kudos