Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5CX Initialization Timing (vl53l5cx_api)

Currently I'm using some of the vl53l5cx api functions along with some custom code. I plan to have multiple ToFs used and noted, via o-scope, that the initialization function vl53l5cx_init (looks to be blocking code?? correct me if I'm wrong) takes a...

JahKMC by Associate III
  • 2910 Views
  • 4 replies
  • 1 kudos

Resolved! Fiber Coupling to remote mount a ToF sensor

Hi I have an application inquiry...'m looking into remote mounting a ToF sensor (i.e. VL53L4EDV0DH/1) in order to observe the environmental limitations of the sensor in a more difficult envorment...are there any guidelines or application history for ...

Resolved! vl53l8cx with SPI interface start ranging fails

To begin, I am using the vl53l8cx breakout board from Pololu with a Nucleo-F446RE and PlatformIO. I have been having trouble getting the VL53L8CX to start ranging using the SPI2 interface. I get successful responses from the `_is_alive()` and `_init(...

lukestroh by Associate II
  • 3163 Views
  • 4 replies
  • 3 kudos

Resolved! VL53L1X temperature effects

We placed two VL53L1X sensors at 18.6" in our temperature chamber. Over a 50C swing we saw up to 1.15" of variability. In the images bellow the chamber temperature stabilized around 30 minutes. The target was a large 24x24 sheet of white nylon 0.5" t...

Brettjohnson7191_0-1733414347663.png

Resolved! VL53L8CX Platform Integration with ChibiOS

Hi, I am trying to integrate the VL53L8CX ULD driver with a project that utilizes chibios on an F4 based board.The TOF sensor firmware seems to be about 86KB. For a transfer of this size, the device fails to setup and use DMA-safe bouncebuffers. I ca...

Resolved! VL53L1X Sensor failures?

#define RANGE_ERROR_DISTANCE_BELOW_DETECTION_THRESHOLD 0x03#define RANGE_ERROR_OTHER 0xFFHi ST,Some of our production devices are receiving the above errors.  Can someone help me with understanding what might cause these errors?Thanks,Will 

will3 by Associate III
  • 1668 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L4CX which distance mode should I choose?

There are three modes: LONG, MEDIUM, and SHORT. The names suggest that LONG allows measuring the greatest distances. In document UM2923 (section 5.2), there is information that the maximum distance can be achieved with the MEDIUM setting. What settin...

Andrew12 by Associate II
  • 5195 Views
  • 9 replies
  • 2 kudos