Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM X-Nucleo-53L7A1 with Nucleo-F401RE does not work

Hi everyone, I have STM Nucleo-F401RE and X-Nucleo-53L7A1. I downloaded the SDK en.X-TOF1. When I check the pin configuration, I saw that X-Nucleo-53L7A1 I2C_RST (PB3) pin is SWO pin on F401RE board at the same time. I needed to delete PB3 pin config...

Ali42_0-1733064280321.png
Ali42 by Associate
  • 1271 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L3CX GUI I2C transaction recording, how?

I have an STM32 Nucleo F401RE plus X-Nucleo-53L3A2 board.IDE and the rest of the toolchain installed, including the STSW-IMG016 P-NUCLEO-53L3A2 pack graphical user interface.The data brief of the GUI states "I2C transaction recording" which is of my ...

Tvan .13 by Associate III
  • 1735 Views
  • 5 replies
  • 1 kudos

Resolved! How manage errors while Init VL53L1X

I'm using the VL53L1X ULD API to drive 4 sensors and, sometimes, the function VL53L1X_SensorInit returns error VL53L1_ERROR_CONTROL_INTERFACE while initializing the third or four sensor (the first two are always initialized correctly).The sensor boot...

nico23 by Senior III
  • 3077 Views
  • 7 replies
  • 2 kudos

Resolved! Best Sensor for Close Readings

We currently use the VL53L1x and have struggled with precise measurements to close objects. Our application needs precise measurements between 1mm and 400mm.  Reviewing the available sensors ST has it appears to us that the VL53L4CD is the best possi...

will3 by Associate III
  • 2663 Views
  • 5 replies
  • 0 kudos

Resolved! Vl53l8 configuring the ranging frequency

Hi,I am using the VL53l8 sensor. i need to change the ranging frequency. im using the Xcube tof code. I see in the app tof code that #define RANGING_FREQUENCY (10U). so if i change 10u to 15. Willi get ranging frequency to 15 hz.? Thank u 

vishnusf by Associate III
  • 1020 Views
  • 1 replies
  • 1 kudos

VL53L8CX Intermittent Stopping Issue

 Hello,I am using the VL53L8CX ToF sensor (I2C) and have encountered an issue. Currently, I’m not using a coverglass, and I have set the sensor to an 8x8 resolution with a frequency of 15 Hz.The problem is that when I run the sensor in an infinite lo...

Short range distance measurement to a point

I'm designing a custom LiDAR sensor for a project and I need a sensor to accurately measure the distance to a small point. I'm looking for an accuracy of +-5mm but the small the better, the maximum range it needs to measure is about 400mm and the min...

esilver by Associate
  • 1386 Views
  • 1 replies
  • 0 kudos