Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L1X and VL53L4CD GetSensorId

Following up on a diff post.  I have a strange result. If I call the GetSensorId for the VL53L1X we use today I get a return of decimal 61098 which is 0xEEAA.  However the comments in the code claim for the GetSensorId should be: "This function retur...

will3 by Associate III
  • 2708 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1X and VL53L4CD detection

We are beginning to migrate from the L1 to the L4.  Wondering if there is a way to auto-detect which sensor is on the board? I would like to build one fw version which abstracts away which sensor is in use (albeit taking advantage of diff features) b...

will3 by Associate III
  • 1986 Views
  • 2 replies
  • 0 kudos

Resolved! ToF sensor with highest sampling frequency

In the search for a distance senor which can sample at highest rate. Given the constraint of a measurement range <1m and accuracy of relative distance changes in the low mm range. Ideally we could get a sampling rate of 1kHz.The VL53L4 sensors would ...

Tom_pm by Associate III
  • 2968 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1X when to trust readings?

Hi,   typedef struct { uint8_t Status; /*!< ResultStatus */ uint16_t Distance; /*!< ResultDistance */ uint16_t Ambient; /*!< ResultAmbient */ uint16_t SigPerSPAD;/*!< ResultSignalPerSPAD */ uint16_t NumSPADs; /*!< ResultNumSPADs */ } VL53L1X_Result_t...

will3 by Associate III
  • 1865 Views
  • 3 replies
  • 2 kudos

Resolved! Sometimes VL6180 is not recognized the object (feat. drift)

Hi ST team,I'm developing the device which is using VL6180. Sometimes ToF(VL6180) is not recognized the object. And sometimes it is not recognized first and then becomes recognized again. But I don't know why this happened. I'm trying to find the rea...

Kyle3 by Associate
  • 1019 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX fails at init

Hello,I am trying to use the VL53L7CX on a robotic project with the provided driver, but it fails at Init.The sensor is detected as alive ("isAlive" is true), the I2C speed is set to 1Mhz (even if I tried lower speeds as well), and it fails exacly at...

Resolved! VL53L8CX data fakes after some time

I am using the VL53L8CX sensor to measure distances, and I am getting correct values. After some time, the data starts to be sometimes incorrect, while slowly increasing the ratio of incorrect vs correct, until eventually all of the readings are inco...

Voklaif by Associate II
  • 1521 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CX not accurate distance

I’ve been using the "vl53l8cx" sensor to measure distances through I2C, and I noticed that when I measure distances (between 10cm and 50cm), the values reported by the sensor are consistently half of the actual distance. For example, when the actual ...