Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

vd55g1 - no data in stream mode

Hi, I'm currently facing a challenge with the VD55G1 driver. I've designed my own minimal system board for the N6 and VD55G1, using MIPI CSI for communication. When attempting to drive the VD55G1, I can enter the stream mode but no data is being tran...

eureka_0-1753080705782.png eureka_1-1753080722856.png eureka_2-1753080734553.png
eureka by Associate II
  • 1364 Views
  • 5 replies
  • 0 kudos

STSW-IMG501 Booting From Script Fails

I am using the STSW-IMG501 software v1.1.1 with the STEVAL-EVK-U0I connected to a STEVAL-56G3MAI (the S-board evaluation module for the VD56G3).  In the EVK software, I am using the built-in script generation tool to upload different register configu...

Resolved! Techniques for multiplexing VL53L4CX

Hi @John E KVAM ... I have seen several discussions about best way to use multiple VL53L4CX sensors, and I've appreciated your responses.  ("Every reboot is its own adventure!").  I'm currently implementing an unusual setup that has 5 of these sensor...

MGG by Associate II
  • 932 Views
  • 2 replies
  • 1 kudos

VL53L5CX Gesture Recognition Implementation on STM32N657

Dear ST Support Team,I hope this message finds you well.I am currently working on a project where I aim to implement gesture recognition using the VL53L5CX sensor. However, I noticed in the official documentation that the supported cores for gesture ...

dw1 by Associate III
  • 1171 Views
  • 2 replies
  • 1 kudos

VL53L4CX Issues

Hello Everyone,We have a custom board that utilizes 10 x VL53L4CX sensors, length of board is about 66cm. For context I am using an NRF54L15 with Zephyr. On bootup they are all configured with a different address and an attempt is made to calibrate t...

imanushev by Associate II
  • 1940 Views
  • 4 replies
  • 0 kudos

Resolved! Wide FoV of upto 120°

Hi, I'm experimenting with VL53L4ED. it suits by requirements except that is has only 18° FoV. Is there any way to increase the FoV (upto120°) using a lens may be without hampering the laser class?

VL53L5CX with Zephyr on NRF Board

Hi everyone, I have been struggling to work with VL53L5CX on my NRF board using Zephyr. I used the VL53L5CX_ULD_driver_2.0.1 API and changed the platform.cpp. So far, what my problem is as follows:Failed on the vl53l5cx_init, because after the firmwa...

osugiw_0-1752315908809.png osugiw_0-1752140817597.png
osugiw by Associate
  • 1258 Views
  • 2 replies
  • 0 kudos