Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Set permanent I2C address to TOF

Hello,I have already use VL53L0X sensor provided by AZ-Delivery.My main problem is that I2C address can be changed but NOT permanently.I am looking to "Adafruit VL53L4CX Time of Flight Sensor". But I don't want to discover the same problem, that is I...

Resolved! [VL53L8CH] Switch between different ranging modes

Dear ST,The VL53L8CH's example codes have demonstrated how the sensor can be controlled through set of APIs. However I am still not very sure about how can I switch between different working modes on-the-fly during runtime.For example, assume I have ...

Rolandash by Associate II
  • 1510 Views
  • 2 replies
  • 1 kudos

Resolved! Ambient light level with vl53l8cx ?

Hello Everyone ! I would like to know if it is possible to measure ambient light levels  either directly or indirectly , using the VL53L8CX sensor. Thank you in advance

kgb by Associate III
  • 2970 Views
  • 8 replies
  • 4 kudos

Resolved! Register Map for VL53L8CX

I am trying to use VL53L8CX with stm32f4 discovery but had no success.  Implementing the preexisitting API has been tough.  Is there a register map for this sensor whcih can be used to create a minimalistic driver and interface sensor using I2C or SP...

Rituraj by Senior
  • 2841 Views
  • 5 replies
  • 2 kudos

Resolved! VL53L4cd not able to detect dark surface

I am trying to use VL53L4CD to detect whether there is a car on top of the sensor or not...I am placing my sensor on the ground and trying to detect if a car is parked on top of the sensor. But it is not able to detect the cars bottom surface. Howeve...

pthakkar by Associate II
  • 1533 Views
  • 6 replies
  • 2 kudos

Resolved! I'm confused about ST nomenclature for VL53L7CH

    I want to try the VL53L7CH, I purchased the SATEL-VL53L7 and the x-nucleo-53l7A1. When I look at the boards on the SATEL-VL53L7 they look identical. But the description says it supports both the CX and CH models. Can someone clear this up?

VD55G0 Video mode

According to the UM2829 manual stating that it supports "SLAVE_I2C STREAMING on I²C pulses", I would like to ask whether this means that image data can be obtained via I2C like the VD55G1, or if it only refers to synchronization signals between image...

eureka by Associate II
  • 1023 Views
  • 4 replies
  • 0 kudos