Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180 can not range longer than 300mm

Hello,It seems the API does not allow to range up to 600mm, why? I am ranging ok up to ~350mm.I have tried to use x3 upscaling, but error is returned when doing so by:VL6180Dev_t    myDevLong;VL6180_UpscaleSetScaling(myDevLong, 3);It seems as upScali...

0693W00000HrhAYQAZ.png
Jhern.1 by Associate II
  • 2238 Views
  • 5 replies
  • 0 kudos

How to detect gesture with VL53L5CX ?

Hello,I'm actually working with the VL53L5CX sensor, i would like to how i can implement gesturedetection like those of the VL53L0 sensor? Do i need more than one ? Is there a specific library ?Thanks for your respons.SL

Slava.1 by Associate
  • 1256 Views
  • 1 replies
  • 0 kudos

VL53L1X sensor address getting reset to 0x29 abrupty

Hi,I'm using the VL53L1X sensor with my raspberry Pi3.Using the python code to read from the two sensors. On starting changing the address using the XSHUT pin.The Pi3 is powered from a battery via regulator. The setup also has an option of being char...

AM.1344 by Associate
  • 1967 Views
  • 2 replies
  • 0 kudos

Resolved! What is the meaning of sigma in L5?

 Hi,I saw in a video (See the screenshot above) that the distance of target is extracted by assuming a normal distribution, and for L5 sensor, we can get sigma (See the second screenshot above).My question is, do the received range sigma means the si...

0693W00000HqrkxQAB.png
Yli.9 by Associate II
  • 1682 Views
  • 2 replies
  • 0 kudos

Resolved! How to use VD6283TX driver?

Hi , Can anyone help to understand how to use the available driver for vd6283TX ambient light sensor as i was able to read the device id and revision id of the device from the driver but the data ready flag is not in a state to read the data,and henc...

BChav.1 by Associate III
  • 1644 Views
  • 1 replies
  • 0 kudos

How large is the Fov of L5's single-zone?

Hi,I am doing extrinsic calibration for VL53L5 and a RGB camera, i.e., i need to locate L5's zones in the RGB image (a zone can be representaed by a quadrilaterals in the RGB image after projection). And my question is: How should i understand the mu...

Yli.9 by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

Has anyone tested the VL53L1X to measure pastures? (pointing down, outdoors, with sunlight from 14 to 93.6 klux)

I´m using multiple sensors for distance ( 3 VL53L1X, 1 HC-SR04, 1 TFMini Plus). I think I need a lot of coverage to shade the measurement point and thus reduce the light to 140 lux (stable in the lab). I tried to switch to short mode and time budget ...

0693W00000HqZMPQA3.jpg 0693W00000HqZhHQAV.jpg 0693W00000HqZiUQAV.jpg

VL53L1X - Timing budget and intermeasurement time

Hi, I´ve been asked for starting new topic for this question.I have general question about speed - in manual, there is line about timing budget which is from 20ms -> 50Hz, but there is InterMeasurement time which is needed to be at least timingBuget ...

0693W000006FLnhQAG.png
VHavl.1 by Associate
  • 2995 Views
  • 1 replies
  • 0 kudos