Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Calibration code for adafruit vl53l0x?

I am planning to place a piece of cover glass over an adafruit vl53l0x sensor connected to an arduino uno. I had a look over the user manual for the vl53l0x and tried using the code provided but it does not work. Is the code not compatible at all for...

MKeun.1 by Associate
  • 1432 Views
  • 1 replies
  • 0 kudos

Does VL53L0X sample code error ?

According the official API code in vl53l0x_api.c , comment says enter standbybut the code was set idle ?Which one is correct ?VL53L0X_Error VL53L0X_StaticInit(VL53L0X_DEV Dev) {   ...   /* Set PAL State to standby */   if (Status == VL53L0...

WLai.2 by Associate
  • 969 Views
  • 1 replies
  • 0 kudos

VL53L0X - How to Interface VL53L0X with PIC18F57Q43?

I interfaced VL53L0X with PIC18F57Q43 and managed to obtain the data, but the sensor requires a hard reset (manually removing the supply and reconnecting it) to obtain continues ranging data. I would like to know how I can obtain the data continuousl...

anusuya by Associate
  • 1135 Views
  • 1 replies
  • 0 kudos

VL53L5CX - access to the ranging histogram

Hi,Is it possible to access the ranging histogram from the zones in the VL53L5. There is a great deal of important information in the histogram which can help enable more powerful applications than just returning peak values.Currently, it does not ap...

JLeav.1 by Associate II
  • 2695 Views
  • 5 replies
  • 0 kudos

VL6180X API Software hints or problems?

Hi,I'm the firmware guy on a project using the VL6180X to detect a person walking up to a machine, and reaching towards it. I have boards here with our processor (MSP430 family) running other parts of the system and it's time to get the VL6180X runni...

Values obtained with range status 2 and 7 are accurate or not?

Hi,I am working on VL53L1X Sensor for designing obstacle detection sensor. When i am testing my sensor's range in office environment, it is showing range status 2 and 7 so frequently even at Timing Budget 140ms. Distance between target and sensor is ...

Akansha by Associate II
  • 1263 Views
  • 1 replies
  • 0 kudos

53L0-SATEL-I1 not working with level shifter ic.

Hi,I am using 53L0-SATEL-I1 with my nxp imx6ul board. This sensor is not working and not detecting on i2c bus address 0x29. I have checked wiring and code all is fine.I am connecting sensor on 10 pin connector and voltage given is 3.3v also checked w...

DChau.2 by Associate
  • 1508 Views
  • 1 replies
  • 0 kudos

Is it wrong that AN5561 shows the distance mode?

I have a question;Recently, I got the sample of VL53L3CX and evaluated the spec with GUI​(STSW-IMG016).According to the AN5561, VL53L3CX seems to have the 3 modes, "Short", "Medium" and "Long".However, I couldn't find the mode option on the GUI.Then ...

TYomo by Associate II
  • 1153 Views
  • 1 replies
  • 0 kudos

VL6180x Accuracy Issue.

Hi Experts and Technical support,We have manufactured 1000 boards with VL6180XV0NR/1 to measure proximity range of 20mm to 80mm. We tested all the boards individually for functionality and accuracy with X-rite white balance card of ~12cm square. Arou...

Vignesh by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos