Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connect multiple VL53L5CX on the same I2C bus of Jetson Nano

Hi, I have a jetson nano and am trying to connect multiple VL53L5CX sensors to its I2C Bus 1. Therefore, I have to update the address for the sensors. According to the documentation, I need to initially pull down all the Lpn pins for the connected se...

MMube.1 by Associate
  • 5714 Views
  • 7 replies
  • 0 kudos

Setup VL53L5 ToF

Hi, I have setup the ToF VL53L5 and started with the simple rangedetektor example in Cube IDE (I'm using the Nucleo STM32F401 board with the X-Nucleo 53L5A1). I'Ve got the message in my serial terminal, that the VL53L5 was not found at the Default I2...

BAAM by Associate
  • 1582 Views
  • 2 replies
  • 1 kudos

VL53L5 Minimum distance setting for "motion indicator"

When using the function "vl53l5cx_motion_indicator_set_distance_motion(&motion_config, min_dis, delta_dis);" One requirement is that "min_dis >=400 mm" . I followed this requirement in my program but, I moved my object in the distance range of "100-...

Yunlion by Associate II
  • 2024 Views
  • 3 replies
  • 0 kudos

Resolved! VD6283 GUI does not calculate the CCT

I have downloaded the VD6283 GUI application and everything works fine except the "Light Spectrum" panel. From the manual I can see that it should calculate the CCT based on the correlation matrix but the CCT window in the top right is always empty. ...

RChit.2 by Associate
  • 1749 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1X ROI (FOV) adjustment question

Hi team,I want to detect an moving object using the VL53L1X sensor.However, there is a problem with the installation angle of the sensor, and we arr looking for a solution.As shown in the above figure, there is interference from a fixed object betwee...

0693W00000JMndbQAD.png 0693W00000JMneZQAT.png
JKim.42 by Associate
  • 3461 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L5 Status code 2, when there is no target

Hello,I have connected a "VL53L5 Satel" board to my Arduino nano BLE board, with modified example code. It works fine with: distance/motion indicator in 4 x 4, continuous mode, ranging frequency 1-10 Hz ( i tried different f). But it only works fine ...

Yunlion by Associate II
  • 1581 Views
  • 2 replies
  • 0 kudos

Usage of VL53L1X for an Electronic Target System

Hi all,​I'm planning on building my own electronic target for pistol shooting - 4.5mm pellets (4.5mmx5mm approx) traveling at 500-600 fps.​I've read the documentation on the L0X and L1X but I'm struggling to figure out if these sensors can fit the bi...

PSilv.3 by Associate
  • 1740 Views
  • 2 replies
  • 0 kudos

Where is VL53L1_PRESETMODE_RANGING defined?

UM2133 says that the available modes are VL53L1_PRESETMODE_RANGING, VL53L1_PRESETMODE_MULTIZONES_SCANNING, VL53L1_PRESETMODE_LITE_RANGING (Obsolete), VL53L1_PRESETMODE_AUTONOMOUS but the only definitions I can find (in API/core/inc/vl53l1_def.h in en...

VL6180 - Interrupt triggered wihoout object ranged

Hello,I am testing the interrupt modes and I have an issue when CONFIG_GPIO_INTERRUPT_LEVEL_HIGH is set to raise the interrut when far objects are detected, but the interrupt is triggered as soon as the continuos mode is started (whit no object in fr...

Jhern.1 by Associate II
  • 1030 Views
  • 1 replies
  • 0 kudos