2022-01-14 2:00 AM
Hello,
I'm actually working with the VL53L5CX sensor, i would like to how i can implement gesture
detection like those of the VL53L0 sensor? Do i need more than one ? Is there a specific library ?
Thanks for your respons.
SL
2022-01-17 10:19 AM
This is a hard question to answer. ST has several patents pending in this area and I can't say anything until after the process is complete - in a couple of months.
But I can say that taking simultaneous 4x4 frames or nearly simultaneous 8x8 frames should be more than enough to do gestures. You will not need another sensor.
The best approach would be to buy the P-nucleo-53L5A1 evaluation kit. You can use it to visualize the data and record the sensor data.
It should only take 2 or 3 frames to establish a target's direction and from there you can work out the motion. Lots of people have taken the data and put it into an A/I engine to get gestures.
Good luck. And I'm sure that ST will make a big splash once the paperwork as been finalized.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.