Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1 Question

Hello.​I2C frequency used by GUI for X-NUCLEO-53L1A2?Can you provide the firmware source used by the GUI for X-NUCLEO-53L1A2?When using the Raning mode of STSW-IMG019 (API for VL53L1CB), is there a minimum requirement for MCU memory, ram, and clock s...

joh.5 by Associate II
  • 1589 Views
  • 1 replies
  • 0 kudos

VL53L1 and VL53L1X Timeing budget

hello.I'm testing the VL53L1 and VL53L1X.When the ambient light is strong, status = 7 is returned.​When the ambient light is strong, how should the timing budget and inter measurement period be set to measure longer distances?​Is it better to acquire...

joh.5 by Associate II
  • 1410 Views
  • 1 replies
  • 0 kudos

VL53L5CX maximum range distance?

Hi,I have some questions about the VL53L5CX maximum range. I am trying to reliably detect an oxygen cylinder passing through a portal 1200mm by 2133mm (floor level). The sensor is mounted at the top of the portal. I can detect cylinder up to approx. ...

MSwan.2 by Associate
  • 1726 Views
  • 1 replies
  • 0 kudos

VL53L0X returns 0x1FFFF (8191)

Hello, I'm using a VL53L0X and it returns 0x1FFFF depending on whether a function within "VL53L0X_StaticInit" is commented or not during initialization. If "VL53L0X_set_reference_spads" is commented, the sensor sends values (with a large offset). But...

0690X00000D96y2QAB.png

Resolved! VL53L5CX LPn pin behavior/usage

I'm testing the VL53L5CX and finding that the behavior of the LPn pin differs from what is described in the datasheet. The datasheet says "Drive this pin to logic 0 to disable the I2C comms when the device is in LP mode. Drive this pin to logic 1 to ...

kwc by Associate III
  • 2150 Views
  • 1 replies
  • 0 kudos